Technical FAQs

Ask a Question

What are the repair parts for an EZM3600FSU, Series M01 main fusible switch unit?

Only the parts listed below are considered field replaceable:

Customer Cover (top compartment) - EZM3600FSUTC
Molded Case Switch Cover (plastic) - BCM
Utility Cover (bottom pull box compartment) - EZM3600FSUBC
Cover Screws - 4020513002K
Molded Case Switch - MHF360006M
Fuses Required (order separately) Class T (300 Vac) 600A max.
Handle extension kit ordered separately - AHEXLI
Keps Nuts (1/2``-13 nut) - 2342702800
Bonding Strap - 7329696753
Mounting Channel - 7329654304
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP

CTA-ID : 5954
Was this helpful?
What can we do to improve the information ?