Technical FAQs

Ask a Question

Are the MAG GARD motor circuit protectors UL489 Listed?

No. MAG GARD`s are UL Recognized Components that comply with NEC requirements for providing motor circuit protection when installed as part of a UL Listed combination controller having motor overload protection.

CTA-ID : 5953
Was this helpful?
What can we do to improve the information ?