Technical FAQs

Ask a Question

What are the repair parts for an EZM1400FSU, Series M01 main fusible switch unit?

Issue:
Previous design repair parts

Product Line:
EZM Metering Equipment

Environment:
Repair parts

Cause:
Maintenance

Resolution:

Only the parts listed below are considered field replaceable:

Customer Cover (top compartment) - EZM1400FSUTC
Molded Case Switch Cover (plastic) - BCM
Utility Cover (bottom pull box compartment) - EZM1400FSUBC
Cover Screws - 4020513002K
Molded Case Switch - LHF26000M
Fuses Required (order separately) Class T (300 Vac) 400A max.
Keps Nuts (1/2``-13 nut) - 2342702800
Bonding Strap - 7329696752
Mounting Channel - 7329654303
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP

 
Was this helpful?
What can we do to improve the information ?