Technical FAQs

Ask a Question

What size screw should be used with the ring tongue terminal on the UL489 listed Multi 9 breaker?

Must use single UL Listed or CSA Certified insulated ring tongue only, with screw 0.2 in. (5 mm); torque 18 lb-in. (2.03 Nm)

CTA-ID : 6171
Was this helpful?
What can we do to improve the information ?