Technical FAQs

Ask a Question

What wire binding torque should be applied when installing a wire with a ring tongue on to the UL489 listed Multi 9 breaker?

Must use single UL Listed or CSA Certified insulated ring tongue only, with screw 0.2 in. (5 mm); torque 18 lb-in. (2.03 Nm)


CTA-ID : 6170
Was this helpful?
What can we do to improve the information ?