Technical FAQs

Ask a Question

What wire binding torque should be applied when installing wire into the UL489 listed Multi 9 breaker?

0.5 to 25 A: #18--#4 AWG (1 to 25 mm^2 ) cables; torque 22 lb-in. (2.48 Nm)
30 to 35 A: #18 to #2 AWG (1 to 35 mm^2 ) cables; torque 31 lb-in. (3.52 Nm)


CTA-ID : 6169
Was this helpful?
What can we do to improve the information ?