Technical FAQs

Ask a Question

How can I keep a UVR from tripping during a brief dip in voltage or momentary loss of power?

The 690UVTD may be set to delay from 0.1 to 0.6 seconds. It works only with the 120Vac UVR, suffix 1121.

CTA-ID : 5502
Was this helpful?
What can we do to improve the information ?