Technical FAQs

Ask a Question

What is the shaft length for the NSF and NSJ door mounted operating handles?

The distance between back of circuit breaker and door are:
NSF: 7.4 to 24 inches (185-600mm)
NSJ: 8.4 to 25 inches (210-625mm)
The shaft can be adjusted by cutting it off.




CTA-ID : 5490
Was this helpful?
What can we do to improve the information ?