Technical FAQs

Ask a Question

Need Mechanical Interlock for interlocking the handles of two 2-Pole or one 2-Pole and one 1-Pole QO and Q1 breakers mounted side by side so that only one breaker can be ``ON`` at a time

Use the QO2DTI


CTA-ID : 5902
Was this helpful?
What can we do to improve the information ?