Technical FAQs

Ask a Question

Is the mushroom button on a XALJ174 control station a maintained device?

Yes it is maintained. A turn to release mushroom button, ZA2BS54, is used in this control station.


CTA-ID : 4976
Was this helpful?
What can we do to improve the information ?