Technical FAQs

Ask a Question

Our customer has an MAL breaker with factory installed 1212 aux. switch and 2100 alarm switch. Can the aux and alarm switches be removed from one MA or MH breaker and installed in another one?<br />

If the bell alarm and aux. switch are a combination device installed in the Right pole, it is not field removeable or installable. If the aux. switch is in the Left pole, it should be easily removed and re-installed. The alarm switch is NOT removeable nor field installable.


CTA-ID : 5473
Was this helpful?
What can we do to improve the information ?