Technical FAQs

Ask a Question

What are the repair parts for a EHB125NS, Series 001 circuit breaker enclosure?

Only the parts listed below are considered field replaceable.
Cover - 4054700701
Cover Mounting Screw - 4020513001K
Neutral Assembly - 4050551450
Neutral Assembly Mounting Screw - 2193817120
Neutral Bonding Hardware - 2100217361
Base Assembly - 4054701050
Base Assembly Mounting Screw - 2190317080
NOTE: Covers and Interior Trims do not have labels applied.

CTA-ID : 6104
Was this helpful?
What can we do to improve the information ?