Technical FAQs

Ask a Question

Is the 9001 K60 padlock attachment OSHA rated lockout tagout ?

No. Locking out a push button is not lockout tagout. It is a control device. For lockout tagout the power must be turned off, locked, and tagged.


CTA-ID : 5167
Was this helpful?
What can we do to improve the information ?