Technical FAQs

Ask a Question

What are the wire binding screw torque requirements for the obsolete CE type breaker?

35 in/lb (14-10 AWG),
40 in/lb (8 AWG),
45 in/lb (6-4 AWG), or
50 in/lb (3-1/0 AWG)



CTA-ID : 5694
Was this helpful?
What can we do to improve the information ?