Technical FAQs

Ask a Question

What is the wire binding torque requirements for the NC100H M9 breaker?<br />

For all amperages, torque is 3.5 N-m or 31.0 lb.-in.


CTA-ID : 5690
Was this helpful?
What can we do to improve the information ?