Technical FAQs

Ask a Question

Need torque specification for lug kit 29229.<br />

The torque specification is 180 lb.-in. for #4AWG-#2AWG Cu cable
180 lb.-in. for #3AWG-#2AWG Al cable
225 lb.-in. for #1AWG - 250kcmil Cu cable and for #1AWG - 350kcmil Al cable.


CTA-ID : 5688
Was this helpful?
What can we do to improve the information ?