Technical FAQs

Ask a Question

Customer is looking C/B # 997000

The 997 series is an ML3 and is replaced by a KAL and SK4516. The SK kit is available through Q2C. For use in ML panels built after 1/1/1962, 31``, 38`` or 46`` wide and 10 5/8`` deep.

CTA-ID : 5681
Was this helpful?
What can we do to improve the information ?