Technical FAQs

Ask a Question

If there is a L in the 3rd position in LAL, MAL, KAL does that means that there are lugs on both ends of the breaker?

Yes.


CTA-ID : 5461
Was this helpful?
What can we do to improve the information ?