Technical FAQs

Ask a Question

Will disconnecting the neutral CT on Micrologic breaker with the ground-fault option -G or LIG or LSG disable or defeat the ground-fault function?

No. Ground fault cannot be disabled on Micrologic breakers. Disconnecting the neutral CT will only make it more likely to trip as all neutral current would be read as ground-fault current.

CTA-ID : 5677
Was this helpful?
What can we do to improve the information ?