Technical FAQs

Ask a Question

What is the replacement for the 997000 series breakers?

These are ML3 breakers which are obsolete, but can be replaced with a KAL breaker and an SK4516 mounting kit. The kit is available for order on Q2C.


CTA-ID : 5617
Was this helpful?
What can we do to improve the information ?