Technical FAQs

Ask a Question

Need a molded case breaker with 65K AIC 200A with walking beam interlock.

The walking beam interlock is not suitable with any breaker that can be rated 65K AIR at 200A.
The MG NSF breakers has the required rating and a handle interlock but the interlock is not UL listed.


CTA-ID : 6084
Was this helpful?
What can we do to improve the information ?