Technical FAQs

Ask a Question

What are the repair parts for an EZM3800FS, Series M01 main fusible switch unit?

Issue:
Design Repair Parts

Product Line:
EZ Metering

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable:

Cover (full length) - EZM3800FSC
Molded Case Switch Cover (plastic) - BCM
Cover Screws - 4020513002K
Molded Case Switch - MHP360008M
Fuses Required (order separately) Class T (300 Vac) 800A max.
Handle extension kit ordered separately - AHEXLI
Standard Lugs for Molded Case Switch (kit includes 1-lug) - AL900MA
Alternate Lugs for Molded Case Switch (kit includes 1-lug) - AL400MA7
Additional Lugs available for Molded Case Switch, refer to Digest
Neutral Lug (kit includes 3-lugs) - MMLK500
Alternate Neutral Lug (kit includes 3-lugs) - MMLK250
Bonding Strap - 7329696750
Mounting Channel - 7329654301
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP

 
Was this helpful?
What can we do to improve the information ?