Technical FAQs

Ask a Question

What are the repair parts for a 92255, Series E1 Double throw Safety Switch?

The parts listed here are the only field replaceable parts.
Blade assembly - 40538-147-50 (does not include lugs)
Top switch base assembly - 40538-142-50 (does not include lugs)
Bottom switch base assembly - 40538-142-50 (does not include lugs)
Handle knob assembly - 40513-001-50
Lug assembly - 40251-147-50 (one lug per blade and base assembly)
Keps nut for mounting lugs - 23427-024-00 (one nut per lug)
base mounting screws - 40206-009-01



CTA-ID : 5850
Was this helpful?
What can we do to improve the information ?