Technical FAQs

Ask a Question

How many operations (on/off) is the UL489 M9 good for?

The UL 489 Multi 9 is good for 6,000 electrical operations at full load, and 4,000 on/off mechanical operations at no load. Total is 10,000.

CTA-ID : 5866
Was this helpful?
What can we do to improve the information ?