Technical FAQs

Ask a Question

What is the part number for an illuminated 2 position maintained red selector switch with no light module and no contacts?

9001 KS11R. A non-illuminated selector switch can be illuminated by removing the square liner on the back of the operator and installing the light module.

CTA-ID : 5124
Was this helpful?
What can we do to improve the information ?