Technical FAQs

Ask a Question

Customer has KAL36225G and GFM250`s Why does it say 250 amp for the GFM250 and the breaker is only rated at 225 amps?

The K frame breaker will go up to 250A which is the max amp breaker that can be used on the GFM250.

CTA-ID : 5653
Was this helpful?
What can we do to improve the information ?