Technical FAQs

Ask a Question

Can a customer use commercially available conductive grease on I-Line jaw connectors?

No. Doing so will void the warranty and will result in deterioration of the bus connection. PJC7201 joint compound is the only product approved for dressing I-Line jaws.
PJC7201 is also used for QMB and MCC. See Supplementary Digest.

CTA-ID : 5426
Was this helpful?
What can we do to improve the information ?