Technical FAQs

Ask a Question

SK4517 Kit and LAL Circuit Breaker in an ML Panelboard

Issue:
How does an LAL branch circuit breaker mount in an ML panelboard?

Product Line:
Obsolete ML panelboards and switchboards sold and supported in the USA in the 1960's.

Environment:
Installation of branch circuit breakers/maintenance.

Cause:
Availability of branch breakers and mounting kits for the obsolete ML panelboards.

Resolution:
Mounting kit number  SK4517 is now obsolete with no replacement.  Consider replacing the panelboard with a new, current I-Line panelboard. 


 
Was this helpful?
What can we do to improve the information ?