Technical FAQs

Ask a Question

What are the repair parts for a NA1200S, Series E01 circuit breaker enclosure?

Only the parts listed below are considered field replaceable.
Cover - 4051551450
Cover Mounting Screw - (8) 4020513001K
Interior Trim - There is no separate Interior Trim used. The cover incorporates a circuit breaker handle access door.
Mounting Pan - 4051526801
Mounting Pan Hardware - (4) 2140422200
Circuit Breaker Lock-Off - HPALM for M frame breaker. HPANA for N frame breaker.
NOTE: Covers do not have labels applied.


CTA-ID : 6062
Was this helpful?
What can we do to improve the information ?