Technical FAQs

Ask a Question

Does option 29450 aux switch comes with NENL34080?

No. It can be ordered separately as 29450, or factory installed with breaker suffix AA. This 29450 number can also be installed to provide a standard alarm switch. Factory installed as BC suffix.

CTA-ID : 5632
Was this helpful?
What can we do to improve the information ?