Technical FAQs

Ask a Question

Customer needs handle mechanism 29338 for an NFNLE36250. Will the shaft extend 9``?

The shaft is 18`` and can be cut to length. The min depth is 185mm max is 600mm back plate to door.

CTA-ID : 5411
Was this helpful?
What can we do to improve the information ?