Technical FAQs

Ask a Question

What are the repair parts for a PAK75CTG, Series E01, ServicePak Power Outlet Panel?

Only the parts listed below are considered field replaceable.
Cover - 4054025101
Cover Mounting Screws - 2142717161
Interior Trim - 4054024501
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - 4054020250 (Does NOT include Base Assembly, see below. Includes Circuit Breaker(s) and Receptacles(s) below.
Base Assembly - 4054008650
Circuit Breaker - QO120GFI, QO130 and QO2505212
Receptacle - 4054001450 (125 volt/20 amp), 4054004450 (125 volt/30 amp) and 4053901901 (Obsolete - Replaced by 4054027950) (125/250 volt/50 amp)
Neutral Bonding Screw - Not Applicable
Note: Covers and Interior Trims do not have labels applied.


CTA-ID : 5406
Was this helpful?
What can we do to improve the information ?