Technical FAQs

Ask a Question

What are the repair parts for a PAK61CT, Series E01, ServicePak Power Outlet Panel?

Only the parts listed below are considered field replaceable.
Cover - 4054025101
Cover Mounting Screws - 2142717161
Interior Trim - 4054025001
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - Not Available. Order Base Assembly, Circuit Breaker(s) and Receptacles(s) below.
Base Assembly - 4054011450
Circuit Breaker - QO120 and (2) QO130
Receptacle - 4054001450 and (2) 4054004450
Neutral Bonding Screw - Not Applicable
Note: Covers and Interior Trims do not have labels applied.


CTA-ID : 5403
Was this helpful?
What can we do to improve the information ?