Technical FAQs

Ask a Question

What are the repair parts for a MA1000R, Series E01 circuit breaker enclosure?

Only the parts listed below are considered field replaceable.
Cover - 4051550350
Cover Mounting Screw - (2) 4510280201
Interior Trim - 4051550401, 4051553701 and (4) 2190317080 (Handles not included, see below)
Interior Trim Handles - (2) 2940101103 and (8) 2142217101
Interior Trim Mounting Screw - (6) 4020513001K
Mounting Pan - 4051553601
Mounting Pan Hardware - (4) 2304528000 and (4) 8010445801
NOTE: Covers and Interior Trims do not have labels applied.


CTA-ID : 6060
Was this helpful?
What can we do to improve the information ?