Technical FAQs

Ask a Question

Why does a trip curve show a lower trip setting than the tables in the Digest?

The Digest table gives the nominal value with a footnote explaining the tolerance. The curve is allowing for the +/- tolerances of 25% on the low setting and 20% on the high.

CTA-ID : 5854
Was this helpful?
What can we do to improve the information ?