Technical FAQs

Ask a Question

Is an early-make contact available for the NSF rotary handle?<br />

Yes, both an early break contact 29345 and early-make contact 29346 is available for the NSF rotary handle. This is also good for the NS100, NS150, and NS250 IEC frames.


CTA-ID : 5847
Was this helpful?
What can we do to improve the information ?