Technical FAQs

Ask a Question

Do we offer an ice cube relay with hermetically sealed contacts?

8501 RS34 is hermetically sealed and is suitable for Class 1 Division 2 locations.


CTA-ID : 5333
Was this helpful?
What can we do to improve the information ?