Technical FAQs

Ask a Question

What are the repair parts for a LA400DS circuit breaker enclosure?

Issue:
Design Repair parts

Product Line:
Circuit Breaker Enclosures

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The only field replaceable parts for this enclosure are the Red/Black handle knobs located on the external operating handle. Part number 4028343950 includes the red knob, black knob and hardware for repair of one handle.


CTA-ID : 6041
Was this helpful?
What can we do to improve the information ?