Technical FAQs

Ask a Question

Can the 9050 JCK25 be used with the initiating contact jumpered and power cycled to reset the device?

No . The contact must be used because the timer must go through a reset program when powered up. If initiating contact is closed during reset, the timer will not work.


CTA-ID : 5309
Was this helpful?
What can we do to improve the information ?