Technical FAQs

Ask a Question

What are the repair parts for a IK250AWK circuit breaker enclosure?

The only field replaceable parts for this enclosure are the Red/Black handle knobs located on the external operating handle. Part number 4028343950 includes the red knob, black knob and hardware for repair of one handle.

CTA-ID : 6038
Was this helpful?
What can we do to improve the information ?