Technical FAQs

Ask a Question

What size of conduit hubs are provided on a KA225X Circuit Breaker Enclosure?

A 2.5`` - 8 NPT hub is provided in the top and bottom endwalls. No other conduit size options are available. The hubs are actually cast as an integral element of the enclosure.


CTA-ID : 5822
Was this helpful?
What can we do to improve the information ?