Technical FAQs

Ask a Question

What is the lug temperature rating on a LEL circuit breaker?<br />

The LEL termination is rated at 75 deg. C.


CTA-ID : 5580
Was this helpful?
What can we do to improve the information ?