Technical FAQs

Ask a Question

What is a KA36225MT35?

This is a top feed I-LINE breaker. MT means the I-LINE jaw connectors are on the OFF end of the circuit breaker, as opposed to the standard location on the ON end. The 35 suffix means it has also been calibrated for 50 deg C ambient instead of the standard 40 deg C.

CTA-ID : 6001
Was this helpful?
What can we do to improve the information ?