Technical FAQs

Ask a Question

What is the combination suffix for a bell alarm (2103), 125Vdc undervoltage release (1129), 50 degree C ambient calibration (35), and factory installed copper lugs (8002)?

That combination suffix is 6188.


CTA-ID : 5989
Was this helpful?
What can we do to improve the information ?