Technical FAQs

Ask a Question

What are the wire binding screw torques for the Compact NSF lugs?

Breaker 15-60A; 106 lb.-in.
Breaker 70-250A: #3 and #2 conductor is 180 lb.-in and #1 to 350 kcmil is 225 lb.-in.


CTA-ID : 5710
Was this helpful?
What can we do to improve the information ?