Technical FAQs

Ask a Question

What is the environmental integrity of a Vario VCF1 or similar ?

The degree of protection is UL/NEMA Type 1 and 12, and IP65.


CTA-ID : 5990
Was this helpful?
What can we do to improve the information ?