Technical FAQs

Ask a Question

Where can I find the wiring diagram for ground fault sensing for the Masterpact NW fixed breaker?

A ground fault sensing wiring diagram for the fixed breaker is in the instruction bulletin provided with the NW breaker. Document number 48049-106-03 page 44.


CTA-ID : 6206
Was this helpful?
What can we do to improve the information ?