Technical FAQs

Ask a Question

Where can I find a wiring diagram for auxiliary connections for the Masterpact NW fixed breaker?

An auxiliary connection wiring diagram for the fixed breaker is in the instruction bulletin provided with the NW breaker. Document number 48049-106-03 page 42 and 43.


CTA-ID : 6203
Was this helpful?
What can we do to improve the information ?