Technical FAQs

Ask a Question

Can we use any other operators than those listed on page 16-115 in Digest 172 in a XACA08 enclosure?

Any of the ZA2 operators can be used. See Digest 171. Do not recommend using the 60mm mushroom buttons because they might interfere with access to next button.


CTA-ID : 4998
Was this helpful?
What can we do to improve the information ?