Technical FAQs

Ask a Question

Where can I find operating conditions like Temperature rerating values for the Masterpact NW?

A temperature rerating table is in the instruction bulletin provided with the NW breaker. Document number 48049-106-03 page 10.


CTA-ID : 6190
Was this helpful?
What can we do to improve the information ?